Hi,
I actually want to establish an Ethernet communication between IMXRT1170 board and my PC. I have seen some driver examples provided in SDK, in that example they used loop back communication and they have defined a mac address in the frame. Now I just want to add an ARP packet in that code so that I can establish communication between the board and my PC. For that I need to give the source MAC address and IP address in ARP packet where IMXRT1170 board is my source. Can anyone please help me by providing any documentation or telling me how to find the mac address and IP address of my board?
Thank you.
Solved! Go to Solution.
Hi
There is a Macro configMAC_ADDR can define the MAC address.
IP address defined by configIP_ADDR
please refer to lwip_ping_bm.c for more details.
Regards
Daniel
Hi
There is a Macro configMAC_ADDR can define the MAC address.
IP address defined by configIP_ADDR
please refer to lwip_ping_bm.c for more details.
Regards
Daniel