How to added pwm support on lnux platform for rt 1052

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to added pwm support on lnux platform for rt 1052

839件の閲覧回数
seven1
Contributor I

HI,

I run rt1052 on linux platform, now need add the pwm function, but not found  the dts & driver file about pwm.please provide releted code .thanks.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

753件の閲覧回数
seven1
Contributor I

Thank you for your reply. This is still the issue. I want to directly write registers on LInux to configure the PWM function, which registers should I configure, and what values should I configure. The more detailed, the better.

This pin is MXRT105X_ PAD_ B1_ 15_ GPIO2_ IO31, mean is MXRT105X_ PAD_ B1_ 15_ FLEXPWM4_ PWMA03。

 

0 件の賞賛
返信

739件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Customer could refer RT1050 SDK software provided PWM demo, which uses eFlexPWM to generate A-phase pwm, B-phase pwm and C-phase pwm through submodule 0, submodule 1, submodule 2. 

Related demo located at ..\SDK_2_13_0_EVKB-IMXRT1050\boards\evkbimxrt1050\driver_examples\pwm

Wish it helps.

best regards,

Mike

0 件の賞賛
返信

824件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Unfortunately, NXP provides MCUXpresso SDK package for RT1050 product, not support ucLinux.

Please check with EmCraft about ucLinux BSP for RT1050.

Wish it helps.

Mike

0 件の賞賛
返信