How to Debugg from SDRAM in imxRT1176

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to Debugg from SDRAM in imxRT1176

4,413 次查看
venkataddagatla
Contributor II

Hi,

I am working on the Imxrt1176 eval board. We recently ported our MQX C++ Project to FREERTOS . Here, I wanted to do debug from SDRAM, I am using MCU expresso IDE. I prepared the debug script to initialize the SDRAM. I am using the Open SDA port for debugging. I can see the breakpoint hitting main after a few minutes where the launching of debugging session halts at 97%  then hits to the main. But after hitting to main I cannot do step debugging(step in). And also there are no class objects are created. 

Kindly let me know if there are any other settings to be done to make successful debugging from SDRAM with openSDA and Jlink.

Kindly review the script files attached for Jlink and opendsda.

Kindly address it early.

Regards,

Venkat Addagatla

 

@kerryzhou @paullaroide @farid_mabrouk 

0 项奖励
回复
10 回复数

4,375 次查看
venkataddagatla
Contributor II

Still, i don't see the Jlink script file in the newly downloaded SDK. It is there with you, kindly share it.

venkataddagatla_0-1631521836121.png

 

0 项奖励
回复

4,372 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @venkataddagatla ,

  Please check my side:

kerryzhou_0-1631524507661.png

Anyway, I attach it.

 

0 项奖励
回复

4,401 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @venkataddagatla ,

   Do you have tested the SDK code, use the JLINK to debug in the SDRAM, whether that is OK or not?

   SDK code already contains: evkmimxrt1170_connect_cm4_cm7side.jlinkscript

  In the JLINKscript, it configure the SDRAM at first, to the debug mode in SDRAM, it also need the script to initialize the SDRAM at first, please try it on your side.

  I use the SDK code and test it with JLINK, it works OK.

  So, you also can follow me to test the SDK led_blinky code with the JLINK debugger at first, then after it works, you can use your mqx porting code.

kerryzhou_2-1631175814433.png

 

kerryzhou_1-1631175807265.png

 

kerryzhou_3-1631175839504.png

 

kerryzhou_4-1631175870241.png

The JLINK script can be found from this link:

SDK_2_10_0_MIMXRT1170-EVK\boards\evkmimxrt1170\demo_apps\led_blinky\cm7\evkmimxrt1170_connect_cm4_cm7side.jlinkscript

Please try it on your side.

If you still have questions about it, please kindly let me know.

Best Regards,

Kerry

0 项奖励
回复

4,392 次查看
venkataddagatla
Contributor II

yes, I will check I get you back for the Jlink script in the SDK.

Before that, my query is how to debug from SDRAM, here from the pics that you have shared that has BOARD_FLASH as a default memory. It means it is debugging from Flash and not from SDRAM.

0 项奖励
回复

4,387 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @venkataddagatla ,

   my laster reply picture 3, select link application to RAM, that already set the code to the secondary one sdram. This is the special good function in the MCUXPresso IDE.

  You also can check the build image, the code is in the SDRAM, you even see my debug result, the code is in the sdram.

 

Best Regards,

Kerry

0 项奖励
回复

243 次查看
burhanhagi
Contributor III

@kerryzhou  I am using ULINK 2 Debugger. I also want to debug my board from external SDRAM.

Actually I did it. I got the same screen as you posted. It runs there. I see 0x8000xxxx address when I halted. Up to here Everything is OK. However, I could not step by step execution code in SDRAM. But  I can easily execute code step by step in QSPI FLash. How will I do the same in SDRAM?

标记 (3)
0 项奖励
回复

224 次查看
burhanhagi
Contributor III

Below is the useful topic tags for anyone who wants to run step by step debugger execution in external SDRAM for imxrt1170;

#Uploading to and executing from SDRAM on the i.MX RT1050 EVK

#RT1170 debugging when application is built for SDRAM

 

 

标记 (3)
0 项奖励
回复

4,382 次查看
venkataddagatla
Contributor II

I have checked in the SDK I couldn't find the Jlink script in the cm7 folder. Kindly can you share the script file here?

venkataddagatla_0-1631515810231.png

 

0 项奖励
回复

4,380 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @venkataddagatla ,

   Your SDK is old, please use the newest sdk SDK2.10.0:

https://mcuxpresso.nxp.com/

Best Regards,

Kerry

0 项奖励
回复

4,236 次查看
nxbg
Contributor I

Hi Kerry,

I download evkmimxrt1170_connect_cm4_cm7side.jlinkscript from your previous attachment inside this topic, but actually the newest 2.10.1 SDK does not have this file actually(I extract the SDK file and search this file but got nothing).

Another problem about this script is that, after download application by following your guide, everything works fine, but if we stop application then click restart(Used very frequencely when we are debugging), then nothing happened, so we need to download again.

nxbg_1-1638187794075.png

Could you help to check a little bit about this small issue?

Thanks & Best Regards,

 

 

 

 

0 项奖励
回复