Hi,
I'm using FlexSPI2 in parallel 16-bit mode @1.8V. The 16 data pins cover 3 power domains: SD_B1, EMC_B2 and unfortunately EMC_B1 for FLEXSPI_B_DATA7 on GPIO_EMC_B1_41. I guess this means that NVCC_EMC1 has to be 1.8V too. (Sigh!) I was hoping to use the GPIO_EMC_B1_XX in non-EMC modes at 3.3V. But it looks like that single FLEXSPI_B_DATA7 on EMC_B1 scuppers that plan and forces the entire set of EMC_B1 pins to be powered at 1.8V. Is there any way around this?
Thanks for your help.
Eamonn
Solved! Go to Solution.
Hello
Hope you are well.
Unfortunately, there is no workaround for this. All the pins linked to that power domain will be 1.8V.
I apologize for the inconvenience this may cause you.
Best regards,
Omar
Hi Omar,
Thank you very much for clarifying this. It is a pity that we have to dedicate all of bank 1 to 1.8V over just one pin, but hey, that's the way they wired it. Thanks again for your help.
Best regards - Eamonn
Hello
Hope you are well.
Unfortunately, there is no workaround for this. All the pins linked to that power domain will be 1.8V.
I apologize for the inconvenience this may cause you.
Best regards,
Omar