Flash driver for GD25LX256

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash driver for GD25LX256

1,437 Views
eamonnheffernan
Contributor III

Hi,

I'm using a GigaDevice GD25LX256 octal nor flash device with a 1051. What flash driver should I select in McuXpresso 11.2? Will MIMXRT1050_SFDP_HYPERFLASH.cfx work? If not, is it difficult to create a custom driver using the Examples/Flashdrivers/NXP/iMXRT projects?

Thanks - Eamonn

0 Kudos
Reply
2 Replies

1,374 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello ,

Hope you are doing well.

I've replied on your other post. For further questions, please respond on the other post to keep the information in one place:

https://community.nxp.com/thread/539365 

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 Kudos
Reply

1,374 Views
jay_heng
NXP Employee
NXP Employee

If you just want a algo for IDE/Tool, you can check my repo imxrt-tool-flash-algo/boards/nxp_evkbmimxrt1050_rev.a1/flash_algo/Keil_JLink at master · JayHeng/imx... 

If you have J-Link, you can easy to build new algo for GD25LX256