The board (MIMXRT1166_EVK) is powered up and connected with a provided USB cable to J11.
When I run Debug I get
MCUXpresso IDE RedlinkMulti Driver v11.4 (Sep 13 2021 15:04:52 - crt_emu_cm_redlink build 16)
Found chip XML file in D:/Workspace_MCUXpresso_11.4/MIMXRT1166_EVK_CM4/Debug\MIMXRT1166xxxxx.xml
Reconnected to existing LinkServer process.
not running connect script in attach mode
Probe Firmware: DAPLink CMSIS-DAP (ARM)
Serial Number: 024400000208827100000000000000000000000097969905
VID:PID: 0D28:0204
USB Path: \\?\hid#vid_0d28&pid_0204&mi_03#9&350958c4&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}
Using memory from core 1 after searching for a good core
Using memory from core 1 after searching for a good core
Using memory from core 1 after searching for a good core
connection failed - Nn(05). Wire ACK Wait in DAP access.. Retrying
Using memory from core 1 after searching for a good core
Using memory from core 1 after searching for a good core
Using memory from core 1 after searching for a good core
Failed on connect: Nn(05). Wire ACK Wait in DAP access
Connected&Reset. Was: NotConnected. DpID: 6BA02477. CpuID: 00000000. Info: <None>
Last stub error 0: OK
Last sticky error: 0x0 AIndex: 1
Debug bus selected: MemAp 1
DAP Speed test unexecuted or failed
Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.
(100) Target Connection Failed
error closing down debug session - Nn(05). Wire ACK Wait in DAP access
What should I set in MCUXpresso IDE or on the board to get it working?
Solved! Go to Solution.
Hi @john71 ,
Please don't worry.
As I know, the MCUXpresso IDE can debug the CM4 core, but you need to download the CM7 at first, that's why I recommend you download the CM7 project, please refer to this post about 2 core debug in mcuxpresso:
Best Regards,
Kerry
Hi @john71 ,
Please download the SDK at first for the RT1160-EVK:
https://mcuxpresso.nxp.com/en/builder?hw=MIMXRT1160-EVK
Then refer to the Getting Started with MCUXpresso SDK for MIMXRT1160-EVK.pdf in folder:
SDK_2_10_0_MIMXRT1160-EVK\docs
You need to download the CM7 project instead of the CM4, and SW1[1:4] should be 0010.
Please try it again.
Wish it helps you!
If you still have questions about it, please kindly let me know.
Best Regards,
Kerry
Hi Kerry,
Thank you for the answer. Frankly - I'm shocked. I need two cores - that's the reason I choose the chip.
What chip do allow us to debug both cores? At design time I can drift to other chip.
Hi @john71 ,
Please don't worry.
As I know, the MCUXpresso IDE can debug the CM4 core, but you need to download the CM7 at first, that's why I recommend you download the CM7 project, please refer to this post about 2 core debug in mcuxpresso:
Best Regards,
Kerry
Thank you. This way it works. If I run CM7 first I can debug CM4 then.