Errors using LPSPI on RT1050 as Slave

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Errors using LPSPI on RT1050 as Slave

1,583件の閲覧回数
peter_lombrozo
Contributor IV

I'm trying to run the LPSPI examples in the SDK (evkbimxrt1050_cmsis_lpspi_int_b2b_transfer_slave) on my EVKB board with a SPI USB emulator (TotalPhase) as Master on my Windows 10.  I'm able to send correct data to the RT1050, but the return data is corrupted.  In addition to using the CMSIS send/receive commands, I've also tried the Transfer command with the same results. Also tried switching from SPI3 to SPI1 channels that are connected to the J24 connector.

When I try to load the TX data buffer for output to the PC Master with anything other than 0's, even the data *sent* to the RT1050 is corrupted.

I saw that the errata for the RT1050 indicated there is an issue if writing to the TCR then writing to the FIFO (ERR011097).  Does this affect the performance of the LPSPI port in the RT1050?

Thanks for any help you can give me.

0 件の賞賛
返信
4 返答(返信)

1,378件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Which SDK version are you using?

0 件の賞賛
返信

1,378件の閲覧回数
peter_lombrozo
Contributor IV

jimmychan->  I'm using 2.4.0, manifest 3.3.0.  I'm realizing now there might be a problem in the USB SPI emulator I'm using where the clock timing is off sending and receiving each bit.  The loopback example (SPI1 <-> SPI3) works.

0 件の賞賛
返信

1,378件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

There is 2.5.0 SDK. Please try the latest version of SDK.

0 件の賞賛
返信

1,378件の閲覧回数
peter_lombrozo
Contributor IV

Yes, did upgrade, no change.  Even sending 1 byte from RT1050 as slave to master only got 4 bits, rest are 0.

0 件の賞賛
返信