Emwin App Wizard 1.08

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Emwin App Wizard 1.08

1,137 次查看
anujtanksali
Contributor II

Hello,

I plan to use the Emwin App wizard for creating my GUI. Am using iMXRT1064 controller.

I have installed the version 1.08 of the APP wizard but I see only BSP for EVK 1050 is currently supported by app wizard. How do I use the app wizard with 1064 controller. 

Thanks

Regards

Anuj

 

 

 

 

0 项奖励
回复
2 回复数

1,055 次查看
nxp16
Contributor III

This did not help.  The emwin documentation says that a bsp needs to have a bspinfo file.  I don't see one in any of the zip files available at that download link, nor in the SDK.  Where do you get a bsp for the 1062 and 1064?

Thanks,

-m

0 项奖励
回复

1,124 次查看
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Please find the more information as the link. URL:https://www.nxp.com/design/software/embedded-software/nxp-emwin-libraries:EMWIN-GRAPHICS-LIBRARY?tab....

Hope it help you. Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 项奖励
回复