EVKB-IMXRT1050 bootloader version

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EVKB-IMXRT1050 bootloader version

1,570 Views
tomars
Contributor II

Hello, 

I have some problem with drag and drop programming (EVKB-IMXRT1050).

I'm using this tutorial:

i.MX RT1050 CMSIS-DAP drag-and-drop programming 

I have two different boards and I dont have any problems with first board - drag and drop programming works fine.

Unfortunately it doesn't work on the second:

pastedImage_1.png

My first board:

pastedImage_1.png

Second:

pastedImage_2.png

On the second - I tried to update the DAPLINK (using this link):

https://www.nxp.com/design/microcontrollers-developer-resources/ides-for-kinetis-mcus/opensda-serial...

Unfortunately I get this error (FAIL.txt):

"The application file format is unknown and cannot be parsed and/or processed."

I think it's the bootloader version problem (version 0244 - drag and drop programming works) - is it possible to update it?

Any other suggestions?

Regards!

Labels (1)
Tags (2)
2 Replies

1,116 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello ,

Hope you are doing well.

Could you please confirm if the revision on both boards is the same?

Also could you please tell me which binary you are downloading from the link so that I may check it from my end.

pastedImage_1.png

You can retry downloading the firmware by keeping in mind the following considerations in the following post:

MCUXpresso IDE V10.1.0 with i.MX RT1052 Crossover Processor | MCU on Eclipse 

Please let me know your results.

Hope it helps!

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

1,116 Views
tomars
Contributor II

It was a problem with boards - first one is the MIMXRT1050- EVK and the second one is the IMXRT1050-EVKB.

0 Kudos
Reply