Do you need RTS and CTS to boot through LPUART1?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Do you need RTS and CTS to boot through LPUART1?

跳至解决方案
1,319 次查看
z_cohen
Contributor I

Hi, we would like to boot through LPUART1. Is is completely necessary to have LPUART1_CTS and LPUART1_RTS? Or can we just use LPUART1_Rx and  LPUART1_Tx?

We're also using ENET and FLEXSPI_A which will block LPUART1_CTS and LPUART1_RTS. We are using the 100-pin LQFP

Thanks,

Zach 

标签 (1)
0 项奖励
回复
1 解答
1,222 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Zach Cohen ,

   Please don't worry, the LPUART boot just need to use UART_TX and UART_RX, it doesn't need the RTS and CTS, so you can use that pin as other function, it's no problem.

  You also can find the boot pin in the RT1020 reference manual:

pastedImage_1.png

Wish it helps you!

If you still have question about it, please kindly let me know.

Have a great day,
Kerry

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

3 回复数
1,223 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Zach Cohen ,

   Please don't worry, the LPUART boot just need to use UART_TX and UART_RX, it doesn't need the RTS and CTS, so you can use that pin as other function, it's no problem.

  You also can find the boot pin in the RT1020 reference manual:

pastedImage_1.png

Wish it helps you!

If you still have question about it, please kindly let me know.

Have a great day,
Kerry

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,222 次查看
z_cohen
Contributor I

Excellent! Thanks a lot 

0 项奖励
回复
1,221 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Zach Cohen,

   You are welcome.

    If your question is solved, please help me to mark the correct answer, just to close this case, thank you!

Wish it helps you!

If you still have question about it, please kindly let me know.

Have a great day,
Kerry

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复