Do I need to use SCCB when I connect a MIPI-CSI camera?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Do I need to use SCCB when I connect a MIPI-CSI camera?

Jump to solution
1,860 Views
Mc2023
Contributor IV

I have a i.MX RT1160 Evaluation Kit and I want to connect a MIPI-CSI camera (AR0144) to the J2 connector.

There is a camera demo provided with the SDK based on the ov5640 camera connected to J2 and uses the SCCB .

Do I need to use SCCB with my AR0144 camera as well? or can I use directly the I2C protocol? Are there any restriction/constraint from the EVK for the protocol to be used?

Br,

0 Kudos
Reply
1 Solution
1,791 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please refer here about Serial Camera Control Bus (SCCB) spec.

Serial Camera Control Bus (SCCB) bus is defined by OmniVision Tech company for control of most functions in OminVision's family of Camera.

Wish it helps.

best regards,

Mike 

View solution in original post

4 Replies
1,824 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

I checked the AR0144 camera supports I2C bus. Customer can use I2C bus communicate with AR0144.

Best regards,

Mike

0 Kudos
Reply
1,804 Views
Mc2023
Contributor IV

Hi,

The OV5640 also supports the I2C. Why are using SCCB and in my case you told me to use I2C?

Best regards,

0 Kudos
Reply
1,792 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please refer here about Serial Camera Control Bus (SCCB) spec.

Serial Camera Control Bus (SCCB) bus is defined by OmniVision Tech company for control of most functions in OminVision's family of Camera.

Wish it helps.

best regards,

Mike 

1,784 Views
Mc2023
Contributor IV

Thanks a lot for your feedback! Now it make sense!

0 Kudos
Reply