Debug on iMXRT1060

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
84件の閲覧回数
seandutoit
Contributor II

Good day

I am having problems programming a imx RT1062 on a custum board.

The question is:

Can I use JTAG/SW debugging if the NVCC_GPIO power group is connected to 1.8V and not 3.3V.

I am using a NXP MCU-Link to debug.

ラベル(1)
0 件の賞賛
返信
1 解決策
34件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @seandutoit,

As mentioned on the Hardware Development User Guide for the RT1060, the NVCC_GPIO power domain should be tied to 3.3V:

EdwinHz_0-1727129981282.png

BR,
Edwin.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
35件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @seandutoit,

As mentioned on the Hardware Development User Guide for the RT1060, the NVCC_GPIO power domain should be tied to 3.3V:

EdwinHz_0-1727129981282.png

BR,
Edwin.

0 件の賞賛
返信
20件の閲覧回数
seandutoit
Contributor II

Thank you for the information

I missed that one.

As all the programming pins are on this bank I guess that will then be the reason why I am having programming problems.

0 件の賞賛
返信