Debug on iMXRT1060

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debug on iMXRT1060

Jump to solution
343 Views
seandutoit
Contributor II

Good day

I am having problems programming a imx RT1062 on a custum board.

The question is:

Can I use JTAG/SW debugging if the NVCC_GPIO power group is connected to 1.8V and not 3.3V.

I am using a NXP MCU-Link to debug.

Labels (1)
0 Kudos
Reply
1 Solution
293 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @seandutoit,

As mentioned on the Hardware Development User Guide for the RT1060, the NVCC_GPIO power domain should be tied to 3.3V:

EdwinHz_0-1727129981282.png

BR,
Edwin.

View solution in original post

0 Kudos
Reply
2 Replies
294 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @seandutoit,

As mentioned on the Hardware Development User Guide for the RT1060, the NVCC_GPIO power domain should be tied to 3.3V:

EdwinHz_0-1727129981282.png

BR,
Edwin.

0 Kudos
Reply
279 Views
seandutoit
Contributor II

Thank you for the information

I missed that one.

As all the programming pins are on this bank I guess that will then be the reason why I am having programming problems.

0 Kudos
Reply