Datasheets of MiMXRT1175AVP8A(144 pin), MiMXRT1175AVJ8A(196 pin)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Datasheets of MiMXRT1175AVP8A(144 pin), MiMXRT1175AVJ8A(196 pin)

ソリューションへジャンプ
533件の閲覧回数
venkat7
Contributor I

Hi,

    I need details of what peripherals available in small form package of  of imxrt1170, they are 

MiMXRT1175AVP8A(144 pin) - 10 x 10 mm

MiMXRT1175AVJ8A(196 pin)  - 12 x 12 mm.

I need what are the peripherals available in the above two packages. I googled them but they are not available.

Please send datasheets/manuals of above both part numbers.

Thank you,

K.Venkatarao.

0 件の賞賛
返信
1 解決策
515件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1) Are they not in production yet?
-- Yes, you can think so.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
526件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
The above two packages are not available, so I'm not assured of they will not contain the peripherals versus MIMXRT1175AVM8A.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
523件の閲覧回数
venkat7
Contributor I

Thank you for your reply.

But as per "i.MX RT1170 Crossover  Processors Data Sheet for Automotive Products".

144, 196 pin configuration available. see below pic, are they not in production yet?

144 pin package RT1175.png

0 件の賞賛
返信
516件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1) Are they not in production yet?
-- Yes, you can think so.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信