DTCM ITCM OCRAM and scatter file on IMX RT1052

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DTCM ITCM OCRAM and scatter file on IMX RT1052

2,666 Views
davidrozenski
Contributor I

Dear All,

I would like to configure at the beginning of my software ITCM 8 Pages, DTCMM 6 pages and OCRAM 2 Pages, so I called the function : FLEXRAM_AllocateRam(&ramAllocate); which is the part of fsl_flexram.c. I defined in the scatter file .scf of KEIL the corresponding regions used :

#define mram_start 0x00000000 // ITCM definition
#define mram_size 0x00040000

#define mram_start1 0x20000000 // DTCM definition
#define mram_size1 0x00030000

#define mram_start2 0x20200000 // OCRAM definition
#define mram_size2 0x00010000

RW_RAM (mram_start) (mram_size ) ;
{

.LONGBUFFER
}

RW_RAM1 (mram_start1) (mram_size1) ;
{

     .ANY (+RW +ZI)
}

in some unit I declared:

volatile uint8_t MyArray[0x30000] __attribute__((section("LONGBUFFER"))) __attribute__ ((aligned(64)));

during linking I got the following message :

MIMXRT1052xxxxx_flexspi_nor_xip_scf(125): warning: L6329W: Pattern *(LONGBUFFER) only matches removed unused sections.

So this is normal since the bank memory definitions (ITCM,DTCM,OCRAM) is done when software started, so how to tell the linker the memory will be usable later ?

Or maybe I missed somethings ?

Regards

David

Labels (1)
0 Kudos
Reply
1 Reply

1,809 Views
igorpadykov
NXP Employee
NXP Employee

Hi David

regarding "how to tell the linker the memory will be usable later ",

discussed in AN 12077 Using the i.MX RT FlexRAM :

As shown in Table 1, there is no valid FlexRAM configuration available in the fuse default setting aligned with the configuration required by this use case. The static configuration cannot be utilized here. However, it is possible to configure the FlexRAM by the run-time configuration approach defined in Section 2.1, “FlexRAM configuration”.

https://www.nxp.com/docs/en/application-note/AN12077.pdf 

For software example one can look at flexram ram allocate example included in  SDK for EVK-MIMXRT1050

https://mcuxpresso.nxp.com/en/dashboard?uvid=71440#

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply