Create a non bootable image on RT1060

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Create a non bootable image on RT1060

ソリューションへジャンプ
821件の閲覧回数
rasm
Contributor I

I have HAB and XIP enabled on RT1060. I would like to use two images, one bootable and one non bootable. The second one would be then loaded from the first one. I can create the bootable image fine with elftosb tool but not the non bootable. How is it possible to create a non bootable image with elttosb (or some other) tool?

0 件の賞賛
返信
1 解決策
810件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Rasm,

We do not have an example with that exact implementation.

You may see on the following Knowledge Base document the steps to generate a bootable image. On of the intermediate steps is generating a binary from your .elf file.

https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/Generating-a-Bootable-Image-for-the-RT1050/ta-p/...

I hope that this information helps!

Regards,
Gustavo

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
811件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Rasm,

We do not have an example with that exact implementation.

You may see on the following Knowledge Base document the steps to generate a bootable image. On of the intermediate steps is generating a binary from your .elf file.

https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/Generating-a-Bootable-Image-for-the-RT1050/ta-p/...

I hope that this information helps!

Regards,
Gustavo

0 件の賞賛
返信