Could the RT1060 Flexspi pin configure to SPI slave mode?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Could the RT1060 Flexspi pin configure to SPI slave mode?

715件の閲覧回数
StephenYeh
Contributor III

Hi Sir

Could the RT1060 Flexspi pin configure to SPI slave mode?

If I use other media for boot device, How to config. Flexspi pin to other mode?(ex: I2C master or slave or SPI slave etc...)

I check the spec., it can't support other function,right?

 

0 件の賞賛
返信
1 返信

710件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi @StephenYeh ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) I check the spec., it can't support other function,right?
-- Yes, it doesn't support.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信