Communication protocol between IMX8 and RT1052

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Communication protocol between IMX8 and RT1052

跳至解决方案
324 次查看
jiaxin
Contributor I

Hi,sir

Requirements:
The system requires data interaction between RT1052 and IMX8, and the wider the rate, the better

What is the maximum bandwidth communication mode between imx8 and RT1052?

0 项奖励
回复
1 解答
244 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

The bandwidth will depend on the protocol used for communication.
You can opt to use LPSPI or ethernet for the communication between devices. 

Best regards,
Omar

在原帖中查看解决方案

0 项奖励
回复
2 回复数
245 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

The bandwidth will depend on the protocol used for communication.
You can opt to use LPSPI or ethernet for the communication between devices. 

Best regards,
Omar

0 项奖励
回复
292 次查看
jiaxin
Contributor I

The amount of data each interaction between the two chips is 512 bytes, and the less time spent, the better

0 项奖励
回复