Clarify: RT1052 ADC external inputs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Clarify: RT1052 ADC external inputs

1,989 次查看
bw1
Contributor IV

The reference manual IMXRT1050RM.pdf states in CH 14: "• Up to 8 single-ended external analog inputs".  However, it appears that more than that are mapped in section "14.2 External Signals".  Also, I am able to assign more than eight when using the Pins Tool (v3.0).  Can you please clarify how many external inputs we can actually connect to ADC inputs via physical pins of the part? 

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,707 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Brad

there are 16 inputs described in Table 4-1. Muxing Options,
sect.14.2 External Signals i.MX RT1050 Reference Manual,

selected by register ADCx_HC0, ADCH: 00000-01111 External channels 0 to 15.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复