Can an i.MX RT EVK Be Used to Program an External MCU Target

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can an i.MX RT EVK Be Used to Program an External MCU Target

682 次查看
vishayp
Contributor I

I see on the i.MX RT 1010 EVK schematic on the section labeled "Freelink" that there are buffers and jumpers on the JTAG/SWD signals. It is unclear, nor can I find any documentation on, if an EVK can be used to program an external design using an MCU in the same family. Can this be done?

If external target programming is possible, should JTAG or SWD be used? What would the connection from an EVK to another MCU look like?

0 项奖励
回复
1 回复

660 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi vishayp,

  The EVK on board debugger SWD interface has two, but one for LPC4322JET100 which is the freemaster own chip, another is the on board target RT1010 chip, so, no directly SWD interface to connect the external target.

  But, from the following picture which is cut from the schematic, you can find the related SWD can be disconnect from the on board target. 

  So, if you want to use the external target, J61, J62 disconnect, then use the related pin1 to connect your external debugger, please also note, you still need to add the VDD, VSS to your external board.

 

kerryzhou_0-1618206523601.png

 

You can try it on your side, but no directly SWD interface.

In fact, I highly suggest you use the external debugger, eg, our LPC-LINK2, MCU-LINK:

https://www.nxp.com/design/microcontrollers-developer-resources/lpc-microcontroller-utilities/lpc-li...

https://www.nxp.com/design/development-boards/lpcxpresso-boards/mcu-link-debug-probe:MCU-LINK

 

Wish it helps you!

Best Regards,

Kerry

 

 

0 项奖励
回复