Hi,
Can RT1170 support MIPI camera like AR1335 CMOS Image Sensor 13 MP?
Is there a limit about the number of pixels in RT1170?
Thanks
解決済! 解決策の投稿を見る。
Hi FYL,
First, please refer to this application notes. https://www.nxp.com/docs/en/application-note/AN5305.pdf
since the MIPI-CSI2 on RT1170 comes from big i.MX devices, it is also useful to evaluate RT1170.
I think it should be okey. For example, when image data is 4K*30fs and YUV422, that is 3840x3160x8bitx30fs=2G. Since RT1170 supports high speed mode (80Mbps - 1.5Gbps) per lane, 4k*30fs can be supported.
Regards,
Jing
Hi FYL,
First, please refer to this application notes. https://www.nxp.com/docs/en/application-note/AN5305.pdf
since the MIPI-CSI2 on RT1170 comes from big i.MX devices, it is also useful to evaluate RT1170.
I think it should be okey. For example, when image data is 4K*30fs and YUV422, that is 3840x3160x8bitx30fs=2G. Since RT1170 supports high speed mode (80Mbps - 1.5Gbps) per lane, 4k*30fs can be supported.
Regards,
Jing