Hello community,
I have one question about BOOT_CFG2[2:0]=000 bit setting for IMXRT1170.
In Reference Manual for IMXRT1050, it have more information about BOOT_CFG2[2:0].
But Reference manual for IMXRT1170 have only minimal information.
Is BOOT_CFG2[2:0]=000b setting is same as RT1050?
I look forward to hearing from you.
Best regards,
Ishii.
Solved! Go to Solution.
Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1)Is BOOT_CFG2[2:0]=000b setting is same as RT1050?
-- Yes, they're almost the same.
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1)Is BOOT_CFG2[2:0]=000b setting is same as RT1050?
-- Yes, they're almost the same.
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hello @jeremyzhou
Thank you for your quick reply.
I will answer it to my customer.
Best regards,
Ishii.