Hi everyone
I have a question about Max Frequency of USDHC1/2_CLK_ROOT.
Q. Is USDHC1/2_CLK_ROOT up to 198MHz?(Sample code and ConfigTools do not match well)
I have using IMXRT1050-EVKB with SDK v2.4.2. And I incorporated the file system with reference to the sample project (EVKB-IMXRT1050\boards\evkbimxrt1050\fatfs_examples\fatfs_sdcard).
According to the sample project the clock setting of USDHC_CLK_ROOT was as follows.
I think that this setting PFD2PFD0 is 528MHz, and USDHC_CLK_ROOT is 528MHz (PFD2PFD0 div 1).
But , In Referrence Manual(pp690), USDHC1/2_CLK_ROOT is up to 198MHz.
In addition, the above values can not be set in ConfigTools.
I tried to some setting as follows.
Best regards,
T.Kashiwagi
已解决! 转到解答。
Hi every one,
Sorry, the reason that SDR 104 does not work properly with IMXRT1050-EVKB was a misconfiguration of PAD.:smileycry:
About IMXRT 1050 - EVKB and IMXRT 1060 - EVK, I confirmed that USDHC_CLK_ROOT works normally at 198 MHz.
So I will mark this comment correctly for the time being.
Measures for this question are as follows.
/* Init System pfd0. */
CLOCK_InitSysPfd(kCLOCK_Pfd0, 16);/* Set USDHC1_PODF. */CLOCK_SetDiv(kCLOCK_Usdhc1Div, 2);/* Set Usdhc1 clock source. */CLOCK_SetMux(kCLOCK_Usdhc1Mux, 1);
#define BOARD_SD_HOST_SUPPORT_SDR104_FREQ (198000000U)
Best Regards,
T.Kashiwagi
Hi every one,
Sorry, the reason that SDR 104 does not work properly with IMXRT1050-EVKB was a misconfiguration of PAD.:smileycry:
About IMXRT 1050 - EVKB and IMXRT 1060 - EVK, I confirmed that USDHC_CLK_ROOT works normally at 198 MHz.
So I will mark this comment correctly for the time being.
Measures for this question are as follows.
/* Init System pfd0. */
CLOCK_InitSysPfd(kCLOCK_Pfd0, 16);/* Set USDHC1_PODF. */CLOCK_SetDiv(kCLOCK_Usdhc1Div, 2);/* Set Usdhc1 clock source. */CLOCK_SetMux(kCLOCK_Usdhc1Mux, 1);
#define BOARD_SD_HOST_SUPPORT_SDR104_FREQ (198000000U)
Best Regards,
T.Kashiwagi
Hi every one,
I experimented with IMXRT 1060-EVK and I will write the result.
· SD_CLK == 198 MHz File Write / Read Verify Test OK!
However, we still need to modify BOARD_SD_HOST_SUPPORT_SDR 104 _ FREQ.
· I used a manufacturer's card different from the time of the experiment of IMXRT 1050-EVKB.
I will confirm next week whether this difference is affecting.
For reference, card performance during testing was as follows.
BS = 8192 [BYTE], WP=10.138389 [MB/S], RP=30.268634 [MB/S]
BS = 16384 [BYTE], WP=20.601566 [MB/S], RP=48.297513 [MB/S]
BS = 32768 [BYTE], WP=19.169942 [MB/S], RP=57.728388 [MB/S]
BS = 65536 [BYTE], WP=19.172698 [MB/S], RP=57.678443 [MB/S]
Best Regards,
T.Kashiwagi
Hi Kashiwagi,
You could take a look at the following Community threads:
https://community.nxp.com/thread/485134
https://community.nxp.com/message/1062302
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Carlos,
Thank you for responding.
I read above Community threads. Thank you bug fix.
But Unfortunately, the above two were about the clock output by USDHC.
USDHC_CLK_ROOT is the clock input to the USDHC module.
my question are What is the correct range of USDHC_CLK_ROOT and When using SDR 104, what is the clock of USDHC_CLK_ROOT? .
I confirmed as follows
Best regards,
T.Kashiwagi
Hi CarlosCasillas and lpcxpresso_support
I found a cause why USDHC does not work. It was caused by BOARD_SD_HOST_SUPPORT_SD104_FREQ and USDHC_SDClock as follows.
In board.h
In fsl_usdhc.h
In case of USDHC_CLK_ROOT == 198MHz, It stopped at the assertion of the 2nd line of USDHC_SDClock
(Because these clocks are busClock_Hz == 200MHz and srcClock_Hz == 198MHz, assertion is correct).
Also I changed BOARD_SD_HOST_SUPPORT_SD104_FREQ to 198000000.
As a result, SD card Initializing copmpleted, But File write/Read verify Test FAILED.
After all, if the sample code is correct, USDHC_CLK_ROOT must be grater than 198 MHz. And if I set USDHC_CLK_ROOT to 198 MHz, it seems that reading and writing of SD card becomes unstable.
I will return to the first question,
Q. how is the correct range of USDHC_CLK_ROOT?
Best Regards,
T.Kashiwagi