AES128 CBC example using DCP and OCOTP key

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AES128 CBC example using DCP and OCOTP key

1,116件の閲覧回数
mb3ddedlov3rs
Contributor I

I'm working on a i.MX RT1052.

I'm trying to run AES128CBC SDK EXAMPLE using DCP and OTP key (SW_GP2) as key, to do this i set DCP_TEST_USE_OTP_KEY to 1 in dcp.c file(from SDK example) and for testing i've written only the first word(32 bit bank 0 bank 5 word 1) of SW_GP2[127:0].

Why when i try to run the software on target the key read from DCP is always 0 ? (I've already check if correctly fused and are ok!) seems that DCP doesn't load the fused key in it's internal memory.

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 返信

1,032件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Customer need to call MCUXpresso SDK provided ocopt driver API function to program OTP fuses.

The OTP fuses default value is 0, the behavior showed OTP key is not programmed.

Customer could refer MCUXpresso [ocotp] demo about how to write data to Fuse map.

Thanks for the attention.


Have a great day,
Mike

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信