1160+1ZM and BT SPP profile

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1160+1ZM and BT SPP profile

2,371件の閲覧回数
kostya740
Contributor II

Hello, I need your help.

I have MIMXRT1160-EVK witn 1ZM M2 WIFI-BT module.
1.png
I was import edgefast_bluetooth/spp example from 2.13 SDK.
Modified define to WIFI_88W8987_BOARD_MURATA_1ZM_M2 in a app_config.h
2.png
Build finished it without any errors.
3.png
Flashed without any errors.
But it is not working. In a terminal, I see only part of output "[sdio] E"
At pin SDIO_CLK I see 400kHz frequency, about 200ms from board start only.
4.jpg

Help me please with this example.

タグ(4)
0 件の賞賛
返信
11 返答(返信)

2,285件の閲覧回数
kostya740
Contributor II

Hi @DanielRuvalcaba 

It is issue when try wifi_cli example. Could you please help?

image.png

0 件の賞賛
返信

2,270件の閲覧回数
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

I’m taking a look into this.

Let me get back to you when I get an update.

 

Regards,

Daniel.

0 件の賞賛
返信

2,250件の閲覧回数
kostya740
Contributor II

Hi @DanielRuvalcaba 

I checked a few points.

1. Is it ok about 400kHz frequency?
2. I have next oscillograms after power on half second.
SDIO CLK

IMG_5819.jpeg
SDIO CMD

IMG_5818.jpeg

3. 

0 件の賞賛
返信

2,181件の閲覧回数
kostya740
Contributor II

@DanielRuvalcaba Hi, doesn't you have any idea?

0 件の賞賛
返信

2,036件の閲覧回数
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi @kostya740,

 

I'm sorry for the late reply.

Could you please tell me if you have removed R183 and added 0ohm resistor at R404 on your board?

 

Regards,

Daniel.

0 件の賞賛
返信

2,013件の閲覧回数
kostya740
Contributor II

Hi,

yes, off course.

0 件の賞賛
返信

1,990件の閲覧回数
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi @kostya740,

 

Could you please send me a picture of your whole setup?

 

Regards,

Daniel.

0 件の賞賛
返信

1,645件の閲覧回数
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi @kostya740,

 

By any chance were you able to get the picture of your whole setup?

 

Regards,

Daniel.

0 件の賞賛
返信

2,135件の閲覧回数
nxf77486
NXP TechSupport
NXP TechSupport

Hello,

 

We are still working on your case, we apologize in advance for the time this will take.

As soon as we have some feedback I would let you know.

0 件の賞賛
返信

2,348件の閲覧回数
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi @kostya740,

 

Could you please help me with the following information?

  • Are you using external power?
  • Are you able to run a Wi-Fi example?
  • Did you do the hardware rework as stated in the Hardware Rework Guide for EdgeFast Bluetooth Protocol Abstraction Layer?

Regards,

Daniel.

 

0 件の賞賛
返信

2,336件の閲覧回数
kostya740
Contributor II

Hi@DanielRuvalcaba 

Thank you for help.

1. Yes. External.
2. I tried. Didn't work too.
3. No. I will do all the need. Thanks.

Do you have another idea? Why didn't BT/WIFI examples work?

0 件の賞賛
返信