Hello,
I want to generate 10khz sine wave and read it back on ADC0 to perturb Battery source. But i am only getting 33 Hz frequency on DAC_out. I am new with the Freedom Boards. I studied some examples in MCUXpresso IDE (SDK 2.6) .Below is the code i am using
Thanks
Solved! Go to Solution.
Hi Farhan Farooq ,
Do you use the PIT to trigger the DAC output?
If yes, what's the PIT frequency you are using? If you want to get the 10khz sine wave, you need to configure the DAC sine data table, then use the PIT to trigger and output it to the DAC, your PIT must more quick than 10Khz, take an example, if one sine wave is divided to 10 points, then your PIT trigger frequency should be 100Khz, so I suggest you test your PIT trigger time is correct or not, then add the DAC code again.
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
BTW, next time, please create your kinetis question to the kinetis forum, this is the RT community, the kinetis forum is :
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thank you for your Reply. i will follow on Kinetis Microcontrollers next time.
I am getting 10.4 khz after i decreases number of samples to 18 per cycle as per following your instruction. my timer value is 5us.
further i will read data through ADC at the same time. so what is your suggestion about that. DAC will send, ADC will Read and processing at the in real time.
Clock Waveform 100khz
DAC output 10khz
this is my code
#define PIT_LED_HANDLER PIT0_IRQHandler
#define PIT_IRQ_ID PIT0_IRQn
/* Get source clock for PIT driver */
#define PIT_SOURCE_CLOCK CLOCK_GetFreq(kCLOCK_BusClk)
void PIT_LED_HANDLER(void)
{
sample = SinusOutputData[is];
is=is+14;
if (is >= SINUS_LENGTH)
{
is = 0;
}
GPIO_PortToggle(BOARD_INITPINS_PTA01_GPIO, 1U << BOARD_INITPINS_PTA01_PIN);
GPIO_PortToggle(BOARD_LED_GPIO, 1u << BOARD_LED_GPIO_PIN);
DAC_SetBufferValue(DEMO_DAC_BASEADDR, 0U, (sample));
pitIsrFlag = false;
/* Clear interrupt flag.*/
PIT_ClearStatusFlags(PIT, kPIT_Chnl_0, kPIT_TimerFlag);
mycount++;
__DSB();
}
/*!
* @brief Main function
*/
int main(void)
{
/* Define the init structure for the output LED pin*/
gpio_pin_config_t led_config = {
kGPIO_DigitalOutput,
0,
};
/*
/* Board pin, clock, debug console init */
BOARD_InitPins();
BOARD_BootClockRUN();
BOARD_InitDebugConsole();
BOARD_InitBootPins();
/* Structure of initialize PIT */
pit_config_t pitConfig;
/*
* pitConfig.enableRunInDebug = false;
*/
PIT_GetDefaultConfig(&pitConfig);
/* Init pit module */
PIT_Init(PIT, &pitConfig);
/* Set timer period for channel 0 */
PIT_SetTimerPeriod(PIT, kPIT_Chnl_0, USEC_TO_COUNT(5U, PIT_SOURCE_CLOCK));
//PIT_SetTimerPeriod(PIT, kPIT_Chnl_0, 500200080);
countValue = USEC_TO_COUNT(5U, PIT_SOURCE_CLOCK);
PRINTF("pit scource clock : %d\r\n", PIT_SOURCE_CLOCK);
PRINTF("total count : %f\r\n", countValue);
/* Enable timer interrupts for channel 0 */
PIT_EnableInterrupts(PIT, kPIT_Chnl_0, kPIT_TimerInterruptEnable);
/* Enable at the NVIC */
EnableIRQ(PIT_IRQ_ID);
/* Start channel 0 */
PRINTF("\r\nStarting channel No.0 ...");
PIT_StartTimer(PIT, kPIT_Chnl_0);
dac_config_t dacConfigStruct;
/* Init output LED GPIO. */
GPIO_PinInit(BOARD_LED_GPIO, BOARD_LED_GPIO_PIN, &led_config);
DAC_GetDefaultConfig(&dacConfigStruct);
DAC_Init(DEMO_DAC_BASEADDR, &dacConfigStruct);
DAC_Enable(DEMO_DAC_BASEADDR, true); /* Enable output. */
while (1)
{
}
}
Hi Farhan Farooq ,
Do you use the PIT to trigger the DAC output?
If yes, what's the PIT frequency you are using? If you want to get the 10khz sine wave, you need to configure the DAC sine data table, then use the PIT to trigger and output it to the DAC, your PIT must more quick than 10Khz, take an example, if one sine wave is divided to 10 points, then your PIT trigger frequency should be 100Khz, so I suggest you test your PIT trigger time is correct or not, then add the DAC code again.
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------