1060 evk12 cannot debug

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1060 evk12 cannot debug

1,463 Views
jingyangxie
Contributor V

I have a board(imxrt1060-evk12) ,when i use the sdk2.12.1 for 1060-evk, it cannot debug with flexspi_nor link file:

jingyangxie_0-1670216875899.jpeg

 

0 Kudos
Reply
5 Replies

1,423 Views
lucas_cao
NXP Employee
NXP Employee

Hi @Alice_Yang  and @jingyangxie 

RT1060 EVK12 used HyperFlash as the boot device. 

So if you are using RT1060's SDK, it makes sense that it cannot work well.

You can try RT1050 SDK becasue it uses HyperFlash as the boot device.

BTW, where did you get the RT1060 EVK12 board? By university program?

 

 

1,453 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @jingyangxie 

It seems there is an issue with the boot jumper:

Alice_Yang_0-1670403158761.png

 

Have a look at :

https://www.nxp.com/document/guide/get-started-with-the-mimxrt1060-evk:GS-MIMXRT1060-EVK  

 

BR

Alice

0 Kudos
Reply

1,436 Views
jingyangxie
Contributor V

I have changed the SW7 to 0010, but it still doesn't work.the log as follows

0 Kudos
Reply

1,429 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @jingyangxie 

Which demo do you run? How about iled_blinky under SDK?

 

BR

Alice

0 Kudos
Reply

1,427 Views
jingyangxie
Contributor V

it can not work too if I use the flexspi_nor.icf link file

0 Kudos
Reply