有關mimxrt685_EVK開發板I2C範例

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

有關mimxrt685_EVK開發板I2C範例

Jump to solution
3,066 Views
DVL
Contributor II

請問mimxrt685_EVK開發板訊號中如輸出SDA與SCL訊號,其level voltage是否能夠調整輸出呢?非常感謝。

0 Kudos
Reply
1 Solution
2,934 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @DVL ,

可以用I2C读写。但是没有范例。

 

Regards,

Jing

View solution in original post

0 Kudos
Reply
11 Replies
3,054 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @DVL ,

这个不能一概而论。I2C信号是open drain的,也就是上管没有输出,只能靠下管导通/关闭。输出电压要靠外部上拉。外部上拉电平需要和这个gpio所在的pin group的供电电压相匹配。有些pin group供电电压是可调的,比如VDDIO_0域的电压可以是1.8V到3.3V。在EVK上有跳线可以选择。

 

Regards,

Jing

0 Kudos
Reply
3,048 Views
DVL
Contributor II

你好,請問mimxrt685_EVK開發版有此範例可以參照實作嗎?會是有文章可以分享,非常感謝。

0 Kudos
Reply
3,032 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @DVL ,

你可以參考一下RT685EVK的Evaluation Board User Manual。其他也沒什麽範例了。

 

Regards,

Jing

0 Kudos
Reply
3,015 Views
DVL
Contributor II

很抱歉,因為使用mimxrt685_EVK開發板所以需要很多地方詢問應用上的問題.

還記得NI的論壇LabView基本上詢問這類應用上的問題,是非常的公開與熱於分享,因為希望大家都使用其產

品,再次感謝,謝謝~

0 Kudos
Reply
3,017 Views
DVL
Contributor II

你好~
很抱歉我沒有獲取到實質的結果,請可以看一下所提的RT685EVK的Evaluation Board User Manual.

其內容再介紹板子,很像沒有實際應用的範例可以供參考?

例如應用上

1.先前提到的VDDIO可以修改其電壓值,請問如何在IDE軟體哪些地方可以進行修改內容呢?

2.使用mimxrt685_EVK開發板將SDA & SCL 訊號直接送給外接至其他裝置上,將所有的I2C範例執行過,皆無法抓取到外接裝置的Slave Address? 我該去哪裡可以詢問或參考外接裝置slave如何接才能正確或軟體設定正確呢?還是我外接裝置端的問題呢?  Evaluation Board User Manual. 沒有範例可以參考正確性.
3.延續上面的mimxrt685_EVK開發板將SDA & SCL 訊號直接送I2C給外接至其他裝置上,是否需要調整boot config為LHH呢?這些應用上的很少可以看到即使手冊上也無詳細說明,或是有手冊有應用方式的手冊呢?

感謝回覆,謝謝.

DVL_0-1670909287625.png

 

 

0 Kudos
Reply
3,002 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @DVL ,

軟體是不可能設電壓值得。你得通過板子上跳綫來設。請綜合datasheet一起看jumper。範例有readme,你再看一下。運行範例需將運行模式設置成L-H-L,FlexSPI Boot from PortB。

EVK的schematic在https://www.nxp.com/downloads/en/design-support/RT685-DESIGNFILES.zip

Regards,

Jing

0 Kudos
Reply
2,991 Views
DVL
Contributor II

你好:

很非常感謝解答,只能使用跳線方式改變電路路經獲取改變電壓.

1.剛剛你建議將”運行範例需將運行模式設置成L-H-L,FlexSPI Boot from PortB“ IDE軟體執行DEBUG馬上出現SPI Flash write error.請參閱附件圖片,

DVL_0-1670920466795.png

2.我目前外接裝置為JESD300-5 SPD5 IC (此IC可以在I2C/I3C下使用),請問boot config需要設定成哪種模式呢? 

3.請問是否能夠提供範例有readme的下載資料,非常感謝.

0 Kudos
Reply
2,976 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi,

1. For sw5, on is LOW, off is HIGH.

2. I'm not familiar with that. I think both are fine.

3. The readme  can be found in the demo's folder, or project->doc.

jingpan_0-1670986354376.png

 

Regards,

Jing

0 Kudos
Reply
2,947 Views
DVL
Contributor II

你好,

最後想請問mimxrt685_EVK開發板是否可以使用I2C 或 I3C 進行EEPROM 讀寫動作呢?
請問是否有其範例可供下載,非常感謝

0 Kudos
Reply
2,935 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @DVL ,

可以用I2C读写。但是没有范例。

 

Regards,

Jing

0 Kudos
Reply
2,974 Views
DVL
Contributor II

非常感謝,很清楚.  ^^

0 Kudos
Reply