yocto x11 with qt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

yocto x11 with qt

3,558件の閲覧回数
sreekanthpk
Contributor I

hai,

         I have been trying to interface a tft display with the imx6q sabreliteboard.I have already configured the board with yocto using  core-image-x11.How can I install qt5 on it ?Can anybody provide the steps for that.Does the core-image-x11 support qt?Or should I bitbake it again with fsl-image-gui?

Thanks in advance

ラベル(2)
0 件の賞賛
3 返答(返信)

1,693件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   NXP BSP contains configuration(s) to build "fsl-image-qt5".

Please refer to BSP documentation for more details.

https://www.nxp.com/webapp/Download?colCode=L3.14.52_1.1.0_LINUX_DOCS&location=null

  Also, the following may be helpful fsl-image-qt5 can support SABRE Lite ? how to config yocto bitbake?


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

1,693件の閲覧回数
sreekanthpk
Contributor I

when i tried fsl-image-qt5 i got error.What shoould I do now ? Does the image availabe to me (that is : bitbake core-image-x11) b not have qt support?

0 件の賞賛

1,693件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

Please refer to qt demo

Regards,

Yuri.

0 件の賞賛