Hi, 心刚
Optional solution:
Most important, Yocto is only a tool chain to build kernel, bootloader or filesystem. If you only want to build 3.0.35 kernel with Yocto, it is simple. But some library, such as QT,GPU, are possibly non-compitable with your kernel.
hi,tao
Thank you for the reply. i have a problem with 3.10.17 on my board, net lose packages(PHY 8031).when i worked with 3.0.35_4.1.0 net was ok
The dora release defaults to 3.0.35-4.1.0. - you can use the branch in community to use Yocto Project with 3.0.35-4.1.0
Daisy branch defaults to 3.10.17-1.0.0 and dizzy branch defaults to 3.10.17-1.0.2