yocto with 3.0.35_4.1.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

yocto with 3.0.35_4.1.0

1,077件の閲覧回数
心刚王
Contributor II

Hi,

     I want use 3.0.35_4.10with yocto project ,what should i do ?

  thanks!

ラベル(7)
0 件の賞賛
返信
3 返答(返信)

860件の閲覧回数
tonyzheng
NXP Employee
NXP Employee

Hi, 心刚

Optional solution:

  1. upgrade kernel to 3.10.17 or upper
  2. downgrade tootchain from Yocto to LTIB

Most important, Yocto is only a tool chain to build kernel, bootloader or filesystem. If you only want to build 3.0.35 kernel with Yocto, it is simple. But some library, such as QT,GPU, are possibly non-compitable with your kernel.

0 件の賞賛
返信

860件の閲覧回数
心刚王
Contributor II

hi,tao

Thank you for the reply. i have a problem with 3.10.17 on my board, net lose packages(PHY 8031).when i  worked with  3.0.35_4.1.0 net was ok


0 件の賞賛
返信

860件の閲覧回数
LaurenPost
NXP Employee
NXP Employee

The dora release defaults to 3.0.35-4.1.0. - you can use the branch in community to use Yocto Project with 3.0.35-4.1.0

Daisy branch defaults to 3.10.17-1.0.0 and dizzy branch defaults to 3.10.17-1.0.2

0 件の賞賛
返信