使用这个配置:
imx-linux-sumo -m imx-4.14.78-1.0.0
DISTRO=fsl-imx-xwayland MACHINE=imx8mmevk source fsl-setup-release.sh -b build-xwayland
使用yocto按照此连https://community.nxp.com/t5/i-MX-Processors/yocto%E5%8D%95%E7%8B%AC%E7%BC%96%E8%AF%91busybox/m-p/1044924,修改源码重新编译,替换文件系统,还是不支持中文。直接使用编译链编译同样版本busybox也是修改同样源码和使用yocto导出.config文件,ls后是能正常显示中文。感觉yocto修改源码,编译没有生效。
You use "bitbake" command and the '-f' option that mean force to compile the busybox. Then use the "bitbake" command and '-f' option to build the whole image again.
e.g.
bitbake busybox -c compile -f
bitbake fsl-image-qt5-validation-imx -f