你好!
yocto版本使用的是V2.4,
配置文件local.conf 内容如下
MACHINE ??= 'imx6qdlsabresd'
2 DISTRO ?= 'fslc-x11'
3 PACKAGE_CLASSES ?= "package_rpm"
4 EXTRA_IMAGE_FEATURES ?= "debug-tweaks"
5 USER_CLASSES ?= "buildstats image-mklibs image-prelink"
6 PATCHRESOLVE = "noop"
7 BB_DISKMON_DIRS ??= "\
8 STOPTASKS,${TMPDIR},1G,100K \
9 STOPTASKS,${DL_DIR},1G,100K \
10 STOPTASKS,${SSTATE_DIR},1G,100K \
11 STOPTASKS,/tmp,100M,100K \
12 ABORT,${TMPDIR},100M,1K \
13 ABORT,${DL_DIR},100M,1K \
14 ABORT,${SSTATE_DIR},100M,1K \
15 ABORT,/tmp,10M,1K"
16 PACKAGECONFIG_append_pn-qemu-native = " sdl"
17 PACKAGECONFIG_append_pn-nativesdk-qemu = " sdl"
18 CONF_VERSION = "1"
在编译imx6Q成功后查看<build dir>/tmp/deploy/images/imx6qdlsabresd目录只有u-boot.img文件,用mfgtool下载固件时的启动文件是u-boot.imx,请问这个文件怎么配置才能编译出来?
Hi Changjing,
The method for compiling u-boot.imx has been described in "i.MX_Linux_User's_Guide.pdf", like below:
---------------------------------------
To build an i.MX 6 or i.MX 7 U-Boot in the standalone environment, find the configuration for the target boot. In the
following example, i.MX 6ULL is the target.
Download source by cloning with git clone http://git.freescale.com/git/cgit.cgi/imx/
uboot-imx.git -b imx_v2017.03_4.9.11-1.0.0_ga
cd uboot-imx
make clean
make mx6ull_14x14_evk_defconfig
make u-boot.imx
-----------------------------------------
So read the user's guide, please!
Have a nice day!
BR,
NXP TIC Weidong Sun