yocto的一些疑问

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

yocto的一些疑问

Jump to solution
2,320 Views
luoyaojun
Contributor II

bitbake生成rootfs后如何删除?每次执行bitbake xxx-image后在deploy目录下都会生成一次rootfs.xxx的文件,如何清除它们?

config/local.conf中IMAGE_INSTALL_append添加的内容无法保存?每次进入编译都需要修改append宏才能生成我要的rootfs?

IMAGE_INSTALL_append += " e2fsprogs" 无法将属于e2fsprogs包的resize2fs命令加入到文件系统?

Labels (1)
1 Solution
2,145 Views
shivanipatel
Senior Contributor II

Hi luoyaojun‌,

Please run below mentioned command to enter in the build directory of the yocto source and check the local.conf file.

  • source setup-environment <build_directory>

You do not need to run the DISTRO = fsl-imx-x11 MACHINE = imx6ulevk source fsl-setup-release .sh -b imx6ul command every time to enter into build directory.

Hope this will help you.

Regards,

Shivani

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
2,145 Views
shivanipatel
Senior Contributor II

Hi luoyaojun‌,

With bitbake -c cleansstate <recipe_name> command you can clear the images in deploy directory generated by bitbake commnad.

The content of added by IMAGE_INSTALL_append in config/local.conf will be saved every time you compile the source with bitbake.

To add the resize2fs command in rootfs, you need to specify below mentioned package in conf/local/conf.

  • IMAGE_INSTALL_append=" e2fsprogs-resize2fs"

Hope this will help you.

Let us know if you have any concern on this.

Regards,

Shivani

0 Kudos
Reply
2,145 Views
luoyaojun
Contributor II

非常感谢:

IMAGE_INSTALL_append=" e2fsprogs-resize2fs"  可以将resize2fs命令加入文件系统。

 bitbake -c cleansstate <recipe_name>, 我使用 bitbake -c cleansstate fsl-image-qt5 无法删除deploy目录下面生成的xxx.ext4, 我用RM_OLD_IMAGE=“1”替代了。

config/local.conf保存问题还是无法实现,比如,我修改了这个文件后,bitbake生成好了image,然后重启虚拟机,重新使用命令STRO=fsl-imx-x11 MACHINE=imx6ulevk source fsl-setup-release.sh -b imx6ul进入,local.conf文件已恢复成我修改之前默认的值了。

0 Kudos
Reply
2,146 Views
shivanipatel
Senior Contributor II

Hi luoyaojun‌,

Please run below mentioned command to enter in the build directory of the yocto source and check the local.conf file.

  • source setup-environment <build_directory>

You do not need to run the DISTRO = fsl-imx-x11 MACHINE = imx6ulevk source fsl-setup-release .sh -b imx6ul command every time to enter into build directory.

Hope this will help you.

Regards,

Shivani

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,145 Views
luoyaojun
Contributor II

谢谢,非常感谢。