wpa supplicant after wifi wlan0 mac change

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

wpa supplicant after wifi wlan0 mac change

1,073 次查看
vladimirchernin
Contributor III

hi!

we are working with imx6ull/ul  and I am trying to change default mac address of wifi wlan0 by using Linux macchanger  app or

ifconfig wlan0 hw ether mac address 

wpa supplicant cannot to connect to access point it cannot get a dhcp address from the server because

its trying to use old mac address.

I dont want to burn mac to efuses and need to do it in software

Thanks

Vladimir

标签 (2)
0 项奖励
回复
1 回复

911 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Vladimir

one can try to use suggestions for changing mac address described in

sect.43.3.2 Getting a MAC Address attached Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复