hi,
currently i am working with the imx6qp sabre ai board. with kernel version 4.1.15. and yocto build.
current issue with detection of usb devices as hidraw.
i can't see the NODE create in /dev as hidraw* . i.e. In the other board : when ever a new hid usb is connected udev creates a node in /dev as /dev/hidraw* and a usb node.
but in over Freescale board that did not work please help me how to resolve this issue..?
Regards,
Lavakumar S
Hi,
Have you ensured the proper USB Host functionality in terms of software (Host driver) and hardware (proper Vbus, connection and grounded ID pin on OTG ports).
You could refer to the following link for additional details:
SABRE|Automotive-Infotainment|i.MX6|NXP
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hi CarlosCasillas,
Thanks for the reply carlos.
Now i understood that we need to enable 'hidraw' and 'hiddev' options in kernel configuration .
What i did is used below commands to work on menuconfig i.e.
bitbake -c ceansstate linux-imx
bitbake -c menuconfig linux-imx
(changed required options)
copied .config to ../source/meta-fsl-arm/recipe-kernel/linux/linux-imx-3.14.38/imx/defconfig
cp /linux-imx/build/.config fsl-release-ivi/source/meta-fsl-arm/recipe-kernel/linux/linux-imx-3.14.38/imx/defconfig
and
bitbake "main core image"
but after building main image i couldn't see the changes on board.
if do : bitbake -c menuconfig linux-imx .
i still can not see the changes.
can someone help to retain the changes made in kernel.
Regards,
Lavakumar S