wm8962 does not work. Based on iMX6dualite

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

wm8962 does not work. Based on iMX6dualite

1,142件の閲覧回数
smithwen
Contributor I

Q: There is no signal output from earphone.

//debug log as below:


imx6qdlsolo login: root
root@imx6qdlsolo:~# cd /
root@imx6qdlsolo:/# aplay 1.wav
wm8962 0-001a: Failed to read DSPCLK: -1
wm8962 0-001a: ASoC: POST_PMU: HPOUTR PGA event failed: -110
wm8962 0-001a: ASoC: POST_PMU: HPOUTL PGA event failed: -110
wm8962 0-001a: Failed to read DCS status: -1
Playing WAVE '1.wav' : Signed 16 bit Little Endian, Rate 44100 Hz, Stereo

タグ(3)
0 件の賞賛
返信
2 返答(返信)

784件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Smith

please check example on

https://community.nxp.com/thread/432057

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

784件の閲覧回数
smithwen
Contributor I

log :


Freescale i.MX Release Distro 3.14.52-1.1.0 imx6qdlsolo /dev/ttymxc0

imx6qdlsolo login: [A
Password:
Login incorrect

imx6qdlsolo login: root
root@imx6qdlsolo:~# cd /
root@imx6qdlsolo:/# aplay 1.wav
wm8962 0-001a: Failed to read DSPCLK: -1
wm8962 0-001a: ASoC: POST_PMU: HPOUTR PGA event failed: -110
wm8962 0-001a: ASoC: POST_PMU: HPOUTL PGA event failed: -110
wm8962 0-001a: Failed to read DCS status: -1
Playing WAVE '1.wav' : Signed 16 bit Little Endian, Rate 44100 Hz, Stereo

0 件の賞賛
返信