Hi
I'm developing custom sabresd board with wm8958.
wm8958 connected via i2s interface with 4 wire (sync mode). AUD3(imx6q) to i2s1(wm8958).
I use imx4.9-imx branch. Enable wm8958 in menuconfig.
In dts use
sound {
compatible = "fsl,imx7d-12x12-lpddr3-arm2-wm8958",
"fsl,imx-audio-wm8958";
model = "wm8958-audio";
audio-codec = <&codec>;
codec-slave;
cpu-dai = <&ssi2>;
asrc-controller = <&asrc>;
mux-int-port = <2>;
mux-ext-port = <3>;
};
codec: wm8958@1a {
compatible = "wlf,wm8958";
reg = <0x1a>;
/*clocks = <&clks IMX6QDL_CLK_CKO>;*/
clocks = <&clks 201>;
clock-names = "mclk1";
wlf,ldo1ena;
wlf,ldo2ena;
i2c-slave;
status = "okay";
};
pinctrl_audmux: audmuxgrp {
fsl,pins = <
MX6QDL_PAD_CSI0_DAT7__AUD3_RXD 0x130b0
MX6QDL_PAD_CSI0_DAT4__AUD3_TXC 0x130b0
MX6QDL_PAD_CSI0_DAT5__AUD3_TXD 0x110b0
MX6QDL_PAD_CSI0_DAT6__AUD3_TXFS 0x130b0
>;
};
&audmux {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_audmux>;
status = "okay";
};
&ssi2 {
assigned-clocks = <&clks IMX6QDL_CLK_PLL4>,
<&clks IMX6QDL_PLL4_BYPASS>,
<&clks IMX6QDL_CLK_SSI2_SEL>;
assigned-clock-parents = <&clks IMX6QDL_CLK_OSC>,
<&clks IMX6QDL_CLK_PLL4>,
<&clks IMX6QDL_CLK_PLL4_AUDIO_DIV>;
assigned-clock-rates = <1179648000>, <0>, <0>;
status = "okay";
};
I use "fsl,imx7d-12x12-lpddr3-arm2-wm8958" becouse there is problem with gpr in linux. Gpr in u-boot is enabled:
CCM_CCGR5, 0x0FFC00C3
In dmesg I saw that wm8958 init.
fsl-ssi-dai 202c000.ssi: No cache defaults, reading back from HW
imx-wm8958 sound: wm8994-aif1 <-> 202c000.ssi mapping ok
ALSA device list:
#0: Loopback 1
#1: wm8958-audio
In alsamixer wm8958 is default, and 100% volume, but sound is off.
I think I have a problem with ssi. How to correct dts?
Hi,
Did you solve this issue finally??
We are also facing the same issue..
We have used imx-wm8958.c machine driver
Which expects some gpr... From dtsi... What to be passed no info... No reference...
I have skipped this gpr parsing in machine driver...
Then ALSA lists that #0 wm8958-audio in boot log....
But no sound is coming out... Probed in oscilloscope... All voltages clks are up... But no sound....
Hi nikita
i.MX7D has not ssi & audmux modules, for ssi & audmux examples on can look
at linux/arch/arm/boot/dts/imx6qdl-sabresd.dtsi
linux-imx.git - i.MX Linux Kernel
May be useful to look at wm8962 driver description in Linux Manual included in
Linux Documentation
https://www.nxp.com/webapp/Download?colCode=L4.9.11_1.0.0_LINUX_DOCS
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
if sound is off, one can check codec signals with oscilloscope and
further debug in codec driver. Refer to Linux Documentation on