Hello all,
I am using sabereSD board based on i.MX6 platform
I wanted to integrate bcm43241 which is of SDIO 3.0 card
when I seen in the sourcecode the /drivers/mmc/sdio/sdio.c is supporting up to CCCR_REV_1.2 only
if it is grater than that it is returning -EINVAL and sdio registration is getting failed
where is my card is CCCR_REV_3_0_0
Did anybody integrated SDIO3.0 wifi card on i.MX6
Kindly let me know if i need to add any patch to support my card
android - 4.2
board- sabereSD
using SD card slot to insert my module mmc1
thanks
Reddy
已解决! 转到解答。
hi, Kernel 3.0 doesn't support SDIO3.0 yet. You can find the SDIO3.0 function supported since Kernel 3.5.7. The attached file is the patch from Kernel 3.5.7 for Kernel 3.0. You can refer to "0002-mmc-recognise-SDIO-cards-with-SDIO_CCCR_REV-3.00.patch" of the attached file, for version check.
Also the SDIO3.0 needs dynamic voltage switch. The circuit must be able to switch voltage between 3.3v and 1.8v, if you are going to apply the attached patches all. Or you can just avoid version check, make your sdio card run with 3.3v only.
hi, Kernel 3.0 doesn't support SDIO3.0 yet. You can find the SDIO3.0 function supported since Kernel 3.5.7. The attached file is the patch from Kernel 3.5.7 for Kernel 3.0. You can refer to "0002-mmc-recognise-SDIO-cards-with-SDIO_CCCR_REV-3.00.patch" of the attached file, for version check.
Also the SDIO3.0 needs dynamic voltage switch. The circuit must be able to switch voltage between 3.3v and 1.8v, if you are going to apply the attached patches all. Or you can just avoid version check, make your sdio card run with 3.3v only.
Thanks for the patch
currently I applied
0002-mmc-recognise-SDIO-cards-with-SDIO_CCCR_REV-3.00.patch
and I am able to maku my wifi module up,
better I will apply entire patch so hat it will meet full functionality
thanks
reddy