wic built image is not booting on the imx8qxp mek board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

wic built image is not booting on the imx8qxp mek board

987 次查看
Poons
Contributor II

Hello,

Yocto Release : Rev. L5.4.24_2.1.0, 06/2020

Machine : imx8mqevk

Distro : fsl-imx-wayland

I built the above release and generated wic image, and image copied to SD card (DD command) and wic image is not booting on the imx8qxp mek board.

but prebuilt wic binaries provided by NXP is boots. kindly help.

Thanks in advance.

Poons

0 项奖励
回复
2 回复数

978 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Poons,

Erase everything and try to do DISTRO=fsl-imx-wayland MACHINE=imx8mqevk source imx-setup-release.sh -b build-wayland
$ bitbake imx-image-multimedia

You must get the wic image similar to the prebuitls images.

 

Regards

 

0 项奖励
回复

923 次查看
Poons
Contributor II

hello,

Thanks for your reply.

I have tried erasing everything & did build, but no success also I noticed that u boot bin size is 730K where as prebuilt u boot size is 1.3M.

 is that u boot not built properly, need any updates? kindly help 

Version of u boot from bb file:
---------------------------------------
UBOOT_SRC ?= "git://source.codeaurora.org/external/imx/uboot-imx.git;protocol=https"
SRCBRANCH = "imx_v2020.04_5.4.24_2.1.0"
SRC_URI = "${UBOOT_SRC};branch=${SRCBRANCH} \
 
Thanks,
Poons
0 项奖励
回复