Hi :
our system start correctly, but the cpu clock only 392000hz,how can i change the cpu freq from ondemand to performance,when I echo performance > /sys/device/system/cpu/cpu0/cpufreq/scalling_setspeed ,it turn out invalid argument.any reply is ok
解決済! 解決策の投稿を見る。
Hi, below is the way to do it suppose the max CPU Frequency is 792 MHz and I want to change from ondemand to performance governor. You can add these lines to any of the init.rc scripts to make these settings
/*Setting the MAX Scaling frequency for CPU*/
echo "7920000" > /sys/devices/system/cpu/cpu0/cpufreq/scaling_max_freq
echo "7920000" > /sys/devices/system/cpu/cpu1/cpufreq/scaling_max_freq
echo "7920000" > /sys/devices/system/cpu/cpu2/cpufreq/scaling_max_freq
echo "7920000" > /sys/devices/system/cpu/cpu3/cpufreq/scaling_max_freq
/*Setting the CPU Freq governor to Performance*/
echo "performance" > /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor
echo "performance" > /sys/devices/system/cpu/cpu1/cpufreq/scaling_governor
echo "performance" > /sys/devices/system/cpu/cpu2/cpufreq/scaling_governor
echo "performance" > /sys/devices/system/cpu/cpu3/cpufreq/scaling_governor
/*Verifying the changes*/
cat /sys/devices/system/cpu/cpu*/cpufreq/scaling_governor
cat /sys/devices/system/cpu/cpu*/cpufreq/scaling_max_freq
I find the answer now, just type make menuconfig , setting the cpu option about freq
using cpu freq driver it is necessary to take care of operating points
supported for specific processor, for example 3 for consumer grade
Table 6
http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf
and 2 for industrial grade
http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQIEC.pdf
Best regards
igor