Hello,
I just meet a simple problem, and I try every method but i still can’t solve it.
I download yocto from http://freescale.github.io/ , and build core-image-base.
MACHINE=imx6ulevk source setup-environment imx6ul
bitbake core-image-base
After it’s finished , I want to remove a module, such as I can see a file
/home/user/fsl-community-bsp/imx6ul/tmp/work/imx6ulevk-poky-linux-gnueabi/core-image-base/1.0-r0/rootfs/lib/modules/4.1.15-1.1.0+ga4d2a08/kernel/drivers/net/wireless/ bcmdhd/ bcmdhd.ko
I just execute “bitbake linux-imx -c menuconfig” and remove this module
“Device Drivers ---> Network device support ---> [ ] Wireless LAN ----”,it’s blank, I didn’t choose it.
And I execute “rm -rf core-image-base” in directory “/home/user/fsl-community-bsp/imx6ul/tmp/work/imx6ulevk-poky-linux-gnueabi”
I wish I won’t see this modules again.
I run commands as below to rebuild.
#!/bin/sh
rm tmp/stamps/imx6ulevk-poky-linux-gnueabi/linux-imx/4.1.15-r0.do_compile*
bitbake linux-imx -c compile
bitbake linux-imx -c compile_kernelmodules
if [ $? -ne 0 ];then
exit
fi
rm sstate-cache/0d/sstate\:linux-imx\:imx6ulevk-poky-linux-gnueabi\:4.1.15\:r0\:imx6ulevk\:3\:0d8abcd98b0d527280499c07fb574e03_deploy.tgz
rm tmp/stamps/imx6ulevk-poky-linux-gnueabi/linux-imx/4.1.15-r0.do_deploy.*
bitbake linux-imx -c deploy
if [ $? -ne 0 ];then
exit
fi
rm tmp/stamps/imx6ulevk-poky-linux-gnueabi/core-image-base/1.0-r0.do_rootfs.*
bitbake core-image-base
but unfortunately, I can find bcmdhd.ko in the same directory.
I just want to know where the cache is.
I even run “rm -rf sstate-cache” to delete all cache directory, but it still there, and the size, the time ,nothing changed.
Anybody tell me where the cache is ?
Thanks very much!
已解决! 转到解答。
I have found the cache and update my script as below:
#!/bin/sh
rm sstate-cache/52/sstate\:linux-fslc-imx\:imx6ulevk-poky-linux-gnueabi\:4.1-1.0.x+gitAUTOINC+0c0844f9fa\:r0\:imx6ulevk\:3\:52f82544cc5787ef98f10d62b5b42468_package.tgz
rm sstate-cache/b2/sstate\:linux-fslc-imx\:imx6ulevk-poky-linux-gnueabi\:4.1-1.0.x+gitAUTOINC+0c0844f9fa\:r0\:imx6ulevk\:3\:b2c1bcfa655e6be4469bffcae4b3bf5c_package_write_rpm.tgz
rm sstate-cache/42/sstate\:linux-fslc-imx\:imx6ulevk-poky-linux-gnueabi\:4.1-1.0.x+gitAUTOINC+0c0844f9fa\:r0\:imx6ulevk\:3\:42c408356014aff14e31711cdc1de51a_packagedata.tgz
rm sstate-cache/ef/sstate\:linux-fslc-imx\:imx6ulevk-poky-linux-gnueabi\:4.1-1.0.x+gitAUTOINC+0c0844f9fa\:r0\:imx6ulevk\:3\:efc8a5ba41ff9e8f6945f6e54f20ef72_deploy.tgz
rm tmp/stamps/imx6ulevk-poky-linux-gnueabi/linux-fslc-imx/4.1-1.0.x+gitAUTOINC+0c0844f9fa-r0.do_compile*
rm tmp/stamps/imx6ulevk-poky-linux-gnueabi/linux-fslc-imx/4.1-1.0.x+gitAUTOINC+0c0844f9fa-r0.do_deploy.*
rm tmp/stamps/imx6ulevk-poky-linux-gnueabi/linux-fslc-imx/4.1-1.0.x+gitAUTOINC+0c0844f9fa-r0.do_package_write_rpm*
rm tmp/stamps/imx6ulevk-poky-linux-gnueabi/linux-fslc-imx/4.1-1.0.x+gitAUTOINC+0c0844f9fa-r0.do_package*
rm tmp/stamps/imx6ulevk-poky-linux-gnueabi/core-image-base/1.0-r0.do_rootfs.*
bitbake linux-fslc-imx -c compile
bitbake linux-fslc-imx -c compile_kernelmodules
if [ $? -ne 0 ];then
exit
fi
bitbake linux-fslc-imx -c deploy
if [ $? -ne 0 ];then
exit
fi
bitbake linux-fslc-imx -c package_write_rpm
if [ $? -ne 0 ];then
exit
fi
bitbake core-image-base
I have found the cache and update my script as below:
#!/bin/sh
rm sstate-cache/52/sstate\:linux-fslc-imx\:imx6ulevk-poky-linux-gnueabi\:4.1-1.0.x+gitAUTOINC+0c0844f9fa\:r0\:imx6ulevk\:3\:52f82544cc5787ef98f10d62b5b42468_package.tgz
rm sstate-cache/b2/sstate\:linux-fslc-imx\:imx6ulevk-poky-linux-gnueabi\:4.1-1.0.x+gitAUTOINC+0c0844f9fa\:r0\:imx6ulevk\:3\:b2c1bcfa655e6be4469bffcae4b3bf5c_package_write_rpm.tgz
rm sstate-cache/42/sstate\:linux-fslc-imx\:imx6ulevk-poky-linux-gnueabi\:4.1-1.0.x+gitAUTOINC+0c0844f9fa\:r0\:imx6ulevk\:3\:42c408356014aff14e31711cdc1de51a_packagedata.tgz
rm sstate-cache/ef/sstate\:linux-fslc-imx\:imx6ulevk-poky-linux-gnueabi\:4.1-1.0.x+gitAUTOINC+0c0844f9fa\:r0\:imx6ulevk\:3\:efc8a5ba41ff9e8f6945f6e54f20ef72_deploy.tgz
rm tmp/stamps/imx6ulevk-poky-linux-gnueabi/linux-fslc-imx/4.1-1.0.x+gitAUTOINC+0c0844f9fa-r0.do_compile*
rm tmp/stamps/imx6ulevk-poky-linux-gnueabi/linux-fslc-imx/4.1-1.0.x+gitAUTOINC+0c0844f9fa-r0.do_deploy.*
rm tmp/stamps/imx6ulevk-poky-linux-gnueabi/linux-fslc-imx/4.1-1.0.x+gitAUTOINC+0c0844f9fa-r0.do_package_write_rpm*
rm tmp/stamps/imx6ulevk-poky-linux-gnueabi/linux-fslc-imx/4.1-1.0.x+gitAUTOINC+0c0844f9fa-r0.do_package*
rm tmp/stamps/imx6ulevk-poky-linux-gnueabi/core-image-base/1.0-r0.do_rootfs.*
bitbake linux-fslc-imx -c compile
bitbake linux-fslc-imx -c compile_kernelmodules
if [ $? -ne 0 ];then
exit
fi
bitbake linux-fslc-imx -c deploy
if [ $? -ne 0 ];then
exit
fi
bitbake linux-fslc-imx -c package_write_rpm
if [ $? -ne 0 ];then
exit
fi
bitbake core-image-base