where is the unit_test tool of i.MX28 ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

where is the unit_test tool of i.MX28 ?

跳至解决方案
888 次查看
9crkzhou
Contributor III

I can't get LRADC run

could someone please tell me where is the unit_test ——no operating system example located ?

please give me a link.

标签 (2)
0 项奖励
1 解答
660 次查看
SergioSolis
NXP Employee
NXP Employee

Please find the OBDS attached.

在原帖中查看解决方案

0 项奖励
4 回复数
660 次查看
GraceH
Senior Contributor II

You can download obds package from freescale.com

IMX_OBDS : On-Board Diagnostic Suit for the i.MX28.

Size (K): 10097 Format: gz Rev #: 1 Modified: 3/3/2011



Grace

0 项奖励
660 次查看
9crkzhou
Contributor III

thanks for your reply,I'v found it.

btw, I can't find the OBDS package of i.MX257.  it doesn't have it in the corresponding place .can you figure it out for me?  thanks a lot.

0 项奖励
661 次查看
SergioSolis
NXP Employee
NXP Employee

Please find the OBDS attached.

0 项奖励
660 次查看
9crkzhou
Contributor III

where did you get that package? I can't find it on the official website.

0 项奖励