where is the unit_test tool of i.MX28 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

where is the unit_test tool of i.MX28 ?

Jump to solution
858 Views
9crkzhou
Contributor III

I can't get LRADC run

could someone please tell me where is the unit_test ——no operating system example located ?

please give me a link.

Labels (2)
0 Kudos
1 Solution
630 Views
SergioSolis
NXP Employee
NXP Employee

Please find the OBDS attached.

View solution in original post

0 Kudos
4 Replies
630 Views
GraceH
Senior Contributor II

You can download obds package from freescale.com

IMX_OBDS : On-Board Diagnostic Suit for the i.MX28.

Size (K): 10097 Format: gz Rev #: 1 Modified: 3/3/2011



Grace

0 Kudos
630 Views
9crkzhou
Contributor III

thanks for your reply,I'v found it.

btw, I can't find the OBDS package of i.MX257.  it doesn't have it in the corresponding place .can you figure it out for me?  thanks a lot.

0 Kudos
631 Views
SergioSolis
NXP Employee
NXP Employee

Please find the OBDS attached.

0 Kudos
630 Views
9crkzhou
Contributor III

where did you get that package? I can't find it on the official website.

0 Kudos