where is dts file for imx6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

where is dts file for imx6

ソリューションへジャンプ
1,358件の閲覧回数
yeyue
Contributor II

I build ltib for imx6 on ubuntu12.04 using package L3.0.35_4.1.0_130816_source.tar.gz

and it can work to produce uboot,kernel image,rootfs

but I can't find any dts files in  rpm/BUILD/linux-3.0.35/arch/arm/boot/

does anyone have ever met this problem?

thanks

0 件の賞賛
返信
1 解決策
980件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

NXP BSP L3.0.35 does not support the Device Tree.


Have a nice day,

Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

3 返答(返信)
981件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

NXP BSP L3.0.35 does not support the Device Tree.


Have a nice day,

Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

980件の閲覧回数
yeyue
Contributor II

Thanks.

If BSP L3.0.35 does not support the Device Tree,

so I need to update BSP for other version?

otherwise how can I change the pinctr in dts file?

0 件の賞賛
返信
980件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

You may try the recent BSP L3.14.52.

http://www.nxp.com/webapp/Download?colCode=L3.14.52_1.1.0_LINUX_DOCS

Summary Page :

i.MX 6 Series Software and Development Tool|NXP

Please follow recommendations of "Freescale_Yocto_Project_User's_Guide.pdf"


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信