when i used i.MX6l boot from emmc, can't mount filesystem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

when i used i.MX6l boot from emmc, can't mount filesystem

1,372 Views
darrenjiao
Contributor I

[    3.715623] mmcblk0: error -84 transferring data, sector 11272, nr 2, cmd response 0x900, card status 0xb00

[    3.725395] mmc2: mmc_rescan_try_freq: trying to init card at 300000 Hz

[    3.732021] mmcblk0: retrying using single block read

[    3.741435] mmc1: Got data interrupt 0x0000000a even though no data operation was in progress.

[    3.752203] mmcblk0: error -84 transferring data, sector 11272, nr 2, cmd response 0x900, card status 0x0

[    3.765848] end_request: I/O error, dev mmcblk0, sector 11272

[    3.776021] EXT3-fs error (device mmcblk0p1): ext3_find_entry: reading directory #2 offset 0

[    3.816229] mmcblk0: error -84 transferring data, sector 11272, nr 2, cmd response 0x900, card status 0xb00

[    3.833410] mmcblk0: retrying using single block read

[    3.859880] mmcblk0: error -84 transferring data, sector 11272, nr 2, cmd response 0x900, card status 0x0

[    3.874579] end_request: I/O error, dev mmcblk0, sector 11272

[    3.900883] EXT3-fs error (device mmcblk0p1): ext3_find_entry: reading directory #2 offset 0

[    3.941341] mmcblk0: error -84 transferring data, sector 11272, nr 2, cmd response 0x900, card status 0xb00

[    3.951106] mmc2: mmc_rescan_try_freq: trying to init card at 200000 Hz

[    3.957765] mmcblk0: retrying using single block read

[    3.969180] mmcblk0: error -84 transferring data, sector 11272, nr 2, cmd response 0x900, card status 0x0

[    3.982822] end_request: I/O error, dev mmcblk0, sector 11272

Labels (1)
0 Kudos
5 Replies

779 Views
igorpadykov
NXP Employee
NXP Employee

Hi Darren

seems eMMC is damaged ("sector 11272, nr 2"), may be recommended to try other.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

779 Views
darrenjiao
Contributor I

Hi Igor,

the emmc device is good, i thinks it's driver issue or i.mx6sl hardware issue, the device I had boot from imx6q success

0 Kudos

779 Views
igorpadykov
NXP Employee
NXP Employee

Hi Darren

device may be bad on this particular sector,

boot image may be located on good sectors.

One can check eMMC read/write (specific "sector 11272, nr 2"")

with SDK:

i.MX 6Series Platform SDK : Bare-metal SDK

~igor

0 Kudos

779 Views
darrenjiao
Contributor I

Hi igor,

you know, I had change some device, and used the i.mx6sl default image, but all failed.

0 Kudos

779 Views
igorpadykov
NXP Employee
NXP Employee

Hi Darren

please try this image on i.MX6SL EVK or

another board

~igor

0 Kudos