[ 3.715623] mmcblk0: error -84 transferring data, sector 11272, nr 2, cmd response 0x900, card status 0xb00
[ 3.725395] mmc2: mmc_rescan_try_freq: trying to init card at 300000 Hz
[ 3.732021] mmcblk0: retrying using single block read
[ 3.741435] mmc1: Got data interrupt 0x0000000a even though no data operation was in progress.
[ 3.752203] mmcblk0: error -84 transferring data, sector 11272, nr 2, cmd response 0x900, card status 0x0
[ 3.765848] end_request: I/O error, dev mmcblk0, sector 11272
[ 3.776021] EXT3-fs error (device mmcblk0p1): ext3_find_entry: reading directory #2 offset 0
[ 3.816229] mmcblk0: error -84 transferring data, sector 11272, nr 2, cmd response 0x900, card status 0xb00
[ 3.833410] mmcblk0: retrying using single block read
[ 3.859880] mmcblk0: error -84 transferring data, sector 11272, nr 2, cmd response 0x900, card status 0x0
[ 3.874579] end_request: I/O error, dev mmcblk0, sector 11272
[ 3.900883] EXT3-fs error (device mmcblk0p1): ext3_find_entry: reading directory #2 offset 0
[ 3.941341] mmcblk0: error -84 transferring data, sector 11272, nr 2, cmd response 0x900, card status 0xb00
[ 3.951106] mmc2: mmc_rescan_try_freq: trying to init card at 200000 Hz
[ 3.957765] mmcblk0: retrying using single block read
[ 3.969180] mmcblk0: error -84 transferring data, sector 11272, nr 2, cmd response 0x900, card status 0x0
[ 3.982822] end_request: I/O error, dev mmcblk0, sector 11272
Hi Darren
seems eMMC is damaged ("sector 11272, nr 2"), may be recommended to try other.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Darren
device may be bad on this particular sector,
boot image may be located on good sectors.
One can check eMMC read/write (specific "sector 11272, nr 2"")
with SDK:
i.MX 6Series Platform SDK : Bare-metal SDK
~igor