I'm looking at the envs in my uboot and here it is:
baudrate=115200 |
bootargs=console=ttymxc0,115200 init=/init video=mxcfb0:dev=hdmi,1920x1080M@60,bpp=32 video=mxcfb1:off video=mxcfb:off video=mxcfb3:off vmalloc=256M androidboot.console=ttymxc0 consolebalank=0 androidboot.hardware=freescale cma=384M
bootcmd=boota mmc1
bootdelay=3
ethact=FEC
ethaddr=00:04:9f:03:ef:39
ethprime=FEC
fastboot_dev=mmc1
fdt_high=0xffffffff
initrd_high=0xffffffff
loadaddr=0x12000000
splashpos=m,m
I don't understand what "bootcmd" values mean. Especially what is 'boota'? I've searched on google and it doesn't give me any meaningful results.
Another question that i have, is that once uboot executes bootcmd, does it automatically execute a kernel initiaing command with 'bootargs' by itself?
Hi chadrick kwag,
The u-boot have two related to the kernel boot environment parameters varialble, they are the bootcmd and bootargs. Here the bootcmd is the commands default start automatically. Bootargs env is an optional setting for booti.
About another question is that once uboot executes bootcmd, does it automatically execute a kernel initiaing command with 'bootargs' by itself? Yes.
Hope this can help you. Any questions contact us easily.
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi chadrickkwag
'boota' is a U-Boot command to boot from an Android boot.img on mmc or from memory.
Here are some infos about boot.img:
https://stackoverflow.com/q/21173628/813810
Try 'help boota' for more details.
Bests,
Diego