while building rootfs with ltib i've encountered a lot of little troubles. finally, i surrender. here's the output:
________________________________________________________________________
Processing: libfslvpuwrap
===========================
Build path taken because: directory build, build key set, no prebuilt rpm,
rpmbuild --dbpath /home/geekay/devel/ltib/rootfs//var/lib/rpm --target arm --define '_unpackaged_files_terminate_build 0' --define '_target_cpu arm' --define '__strip strip' --define '_topdir /home/geekay/devel/ltib/rpm' --define '_prefix /usr' --define '_tmppath /home/geekay/devel/ltib/tmp' --define '_rpmdir /home/geekay/devel/ltib/rpm/RPMS' --define '_mandir /usr/share/man' --define '_sysconfdir /etc' --define '_localstatedir /var' -bc --short-circuit /home/geekay/devel/ltib/dist/lfs-5.1/fsl-mm/libfslvpuwrap.spec
Building target platforms: arm
Building for target arm
Executing(%build): /bin/sh -e /home/geekay/devel/ltib/tmp/rpm-tmp.62833
+ umask 022
+ cd /home/geekay/devel/ltib/rpm/BUILD
+ cd libfslvpuwrap-1.0.35
+ which pkg-config
+ export PKG_CONFIG=/opt/freescale/ltib/usr/bin/pkg-config --static
+ ./configure --prefix=/usr --host=arm-linux --build=x86_64-unknown-linux-gnu
checking for a BSD-compatible install... /usr/bin/install -c
checking whether build environment is sane... yes
checking for arm-linux-strip... arm-linux-strip
checking for a thread-safe mkdir -p... /bin/mkdir -p
checking for gawk... gawk
checking whether make sets $(MAKE)... yes
checking whether to enable maintainer-specific portions of Makefiles... no
checking pkg-config is at least version 0.9.0... yes
checking for style of include used by make... GNU
checking for arm-linux-gcc... gcc
checking whether the C compiler works... yes
checking for C compiler default output file name... a.out
checking for suffix of executables...
checking whether we are cross compiling... yes
checking for suffix of object files... o
checking whether we are using the GNU C compiler... yes
checking whether gcc accepts -g... yes
checking for gcc option to accept ISO C89... none needed
checking dependency style of gcc... gcc3
checking for library containing strerror... none required
checking for arm-linux-gcc... (cached) gcc
checking whether we are using the GNU C compiler... (cached) yes
checking whether gcc accepts -g... (cached) yes
checking for gcc option to accept ISO C89... (cached) none needed
checking dependency style of gcc... (cached) gcc3
checking for arm-linux-gcc... (cached) gcc
checking whether we are using the GNU C compiler... (cached) yes
checking whether gcc accepts -g... (cached) yes
checking for gcc option to accept ISO C89... (cached) none needed
checking dependency style of gcc... (cached) gcc3
checking how to run the C preprocessor... gcc -E
checking for grep that handles long lines and -e... /bin/grep
checking for egrep... /bin/grep -E
checking for ANSI C header files... yes
checking build system type... x86_64-unknown-linux-gnu
checking host system type... arm-unknown-linux-gnu
checking how to print strings... printf
checking for a sed that does not truncate output... /bin/sed
checking for fgrep... /bin/grep -F
checking for ld used by gcc... ld
checking if the linker (ld) is GNU ld... yes
checking for BSD- or MS-compatible name lister (nm)... /opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-linux-nm -B
checking the name lister (/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-linux-nm -B) interface... BSD nm
checking whether ln -s works... yes
checking the maximum length of command line arguments... 1572864
checking whether the shell understands some XSI constructs... yes
checking whether the shell understands "+="... yes
checking how to convert x86_64-unknown-linux-gnu file names to arm-unknown-linux-gnu format... func_convert_file_noop
checking how to convert x86_64-unknown-linux-gnu file names to toolchain format... func_convert_file_noop
checking for ld option to reload object files... -r
checking for arm-linux-objdump... arm-linux-objdump
checking how to recognize dependent libraries... pass_all
checking for arm-linux-dlltool... no
checking for dlltool... no
checking how to associate runtime and link libraries... printf %s\n
checking for arm-linux-ar... ar
checking for archiver @FILE support... @
checking for arm-linux-strip... (cached) arm-linux-strip
checking for arm-linux-ranlib... arm-linux-ranlib
checking command to parse /opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-linux-nm -B output from gcc object... ok
checking for sysroot... no
checking for arm-linux-mt... no
checking for mt... mt
configure: WARNING: using cross tools not prefixed with host triplet
checking if mt is a manifest tool... no
checking for sys/types.h... yes
checking for sys/stat.h... yes
checking for stdlib.h... yes
checking for string.h... yes
checking for memory.h... yes
checking for strings.h... yes
checking for inttypes.h... yes
checking for stdint.h... yes
checking for unistd.h... yes
checking for dlfcn.h... yes
checking for objdir... .libs
checking if gcc supports -fno-rtti -fno-exceptions... no
checking for gcc option to produce PIC... -fPIC -DPIC
checking if gcc PIC flag -fPIC -DPIC works... yes
checking if gcc static flag -static works... yes
checking if gcc supports -c -o file.o... yes
checking if gcc supports -c -o file.o... (cached) yes
checking whether the gcc linker (ld) supports shared libraries... yes
checking whether -lc should be explicitly linked in... no
checking dynamic linker characteristics... GNU/Linux ld.so
checking how to hardcode library paths into programs... immediate
checking whether stripping libraries is possible... yes
checking if libtool supports shared libraries... yes
checking whether to build shared libraries... yes
checking whether to build static libraries... yes
checking vpu_lib.h usability... no
checking vpu_lib.h presence... no
checking for vpu_lib.h... no
configure: error: lib_vpu is required, consider installing imx-lib
error: Bad exit status from /home/geekay/devel/ltib/tmp/rpm-tmp.62833 (%build)
RPM build errors:
Bad exit status from /home/geekay/devel/ltib/tmp/rpm-tmp.62833 (%build)
Build time for libfslvpuwrap: 3 seconds
Failed building libfslvpuwrap
____________________________________________________________________________________________
what am i doing wrong? didn't find much in the internet about this problem
i use kernel 3.0.35 from wandboard and build rootfs with ltib 4.1.0. the host system is debian 7.1
Konstantin
Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel
free to reply with an update to this discussion.
Thanks,
Yixing
Hello,
I've got the same issue. Did you find a workaround ?
Regards
Alexandre Schnegg
Make sure you have the packate imx-lib selected, under the package list, on the ltib's menuconfig.
it's selected, compiled and packed in /opt/freescale/pkgs. how ca i make myself sure that ltib is linking the library?
Not sure what is going on. Are you having the same problem or a linking problem? Can you please start with a FSL GNOME package profile? (./ltib -m selectype).