Hi community,
I want to confirm how to set i.MX6 FCB values for NAND.
Please see Table 8-12 in IMX6SDLRM (Rev.1) and my questions as below.
[Q1]
At first I want to confirm whether FCB is unique data for i.MX series or not.
Could you let me know it?
[Q2]
The unit of m_NandTiming values are "nano seconds" as per NAND datasheet.
So I should program "0x0A" to m_NandTiming if the correspondent value in NAND datasheet is "10 ns".
Is my understanding correct?
[Q3]
As per NAND datasheet, REA, RLOH, and RHOH values are written as max value.
Should I program the max values to m_NnandTiming[7:5]?
[Q4]
I want to confirm what is "dsample_time" and "nand_timing_state".
What parameters in NAND datasheet are corresponded them?
[Q5]
To disable "Onfi_sync_enable", should I set it to 0x00000000?
Best Regards,
Satoshi Shimoda
解決済! 解決策の投稿を見る。
Hi Satoshi Shimoda,
Have you ever tried our MFG tool, in the MFG tool there is a "kobs-ng" tool will flash the FCB to the NAND.
So you no need be aware of it.
BR
Justin
Satoshi
Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help please feel 
free to contact Freescale.
Thanks,
Yixing
Hi Yixing Kong,
Yes, our issue has been resolved.
It is OK because I will use MFG-Tool for NAND programming.
Best Regards,
Satoshi Shimoda
Hi Satoshi Shimoda,
Have you ever tried our MFG tool, in the MFG tool there is a "kobs-ng" tool will flash the FCB to the NAND.
So you no need be aware of it.
BR
Justin
Could anyone reply me?